Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C123GH6PM: Problem IN SMBus communication Using SMSbuc.c and SMBus.h from Utils...

Part Number: TM4C123GH6PM

Tool/software: TI-RTOS

I tried to communicate using smbus on tm4c123gh6pm. Hrer is my code. I does not receive in g_pucSlaveRxBuffer.  

void SMBusInitonI2C(void) {


//
// Enable the peripherals for the SMBus master.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Configure the required pins for I2C0.
//
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOB))
{
}
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
//
// Configure the IO mux so that the I2C pins for I2C0 are on PB2/3.
//

//
// Initialize the master SMBus port.
//
SMBusMasterInit(&g_sMaster, I2C0_BASE, SysCtlClockGet());

I2CIntRegister(GPIO_PORTB_BASE,&SMBusMasterIntHandler);
// Enable master interrupts.
//
SMBusMasterIntEnable(&g_sMaster);
I2CMasterEnable(I2C0_BASE);
IntMasterEnable();

}

U8_t readFromSlave(U8_t device_address, U8_t device_register) {

int i;

SMBusPECEnable(&g_sMaster);

returnStatus = SMBusMasterByteWordRead(&g_sMaster, device_address, device_register, g_pucSlaveRxBuffer, 2);
 UARTprintf("Status: %d \r\n",returnStatus);

for(i=0; i<2; i++) {

UARTprintf("%d \r\n",g_pucSlaveRxBuffer[i]);

}

return 0;

}

 If anyone has done SMBus communication please help me...