Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: Problem in UART communication while interfacing HC05 with the Launchpad

Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: TM4C123GH6PM, ENERGIA

Hello.

I have been trying to create a serial link between the Launchpad (based on tm4c123gh6pm) and my cellphone. The code is very simple for testing purpose. Here is it:

/* This is a demo code for testing Bluetooth functionality 
->The peripheral used here was a smartphone; and to obtain the values of 'i' on the terminal of the device, the "display mode" setting must be changed to ' HEX' 
->The code doesn't work properly on when the pin 10 and 11 are used as RX and TX
->It has been successfully tested to send the values of i to the Rx terminal and receive the characters sent from there. */

int i=0;
void setup()
{
 Serial.begin(9600);
 Serial.print("Welcome ");
}

 char data_from_Blue=0;
 //String rx_str = "";
 
void loop() 
{
   for(i=0;i<10;i++)
   {
        if(Serial.available()>0)
        {  
           data_from_Blue = Serial.read();    // reading the data received from the bluetooth module/the peripheral (phone here)          
           Serial.println("I received: ");
           Serial.println(data_from_Blue);
           //Serial.println(rx_str);   //display it on serial monitor  i.e,the reading has been received here!!               
        }
  
      Serial.write(i);                //Print incrementing value of 'i' across the other terminal(i.e, my cellphone) 
      delay(1000);
   }   
}

The code works fine for Arduino+HC05 and MSP430G2 Lauchpad Kit+HC05.

But for TIVA Launchpad mentioned above, the serial monitor simply displays garbled values with '?' within boxes. I have tried almost everything.

Please help me.