This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LC4357: TMS570LC4357 HDK EMIF_DATA

Part Number: TMS570LC4357

Tool/software: Code Composer Studio

Which ball is routed to J10 from HDK?

Several balls are not consistent of the datasheet of TMS570 and HDK (EMIFDATA N2HET2)

eg: ball T8 N2HET2[23] from datasheet and ball EMIFDATA[15] from HDK Userguide

TMS570 datasheet

HDK Userguide

Thank you

Dieter

  • Hello Dieter,
    According to TMS570LC43x HDK schematic diagram, balls K16, L16, M16, N16, E4, F4, G4, K4, L4, M4, N4, P4, T5, T6, T7 and T8 are not connected. Also in schematic diagram, ball/signal names of those balls differs from Datasheet (they are same as in User Guide). I'll double check about this discrepancy.
    Datasheet is the primary document we are referring to.
    You can follow the connection ofJ10 in schematic diagram which could be found here: www.ti.com/.../tmdx570lc43hdk

    Best regards,
    Miro

  • Hello Dieter,
    Please refer to Datasheet for K16, L16, M16, N16, E4, F4, G4, K4, L4, M4, N4, P4, T5, T6, T7 and T8 ball names.

    Best regards,
    Miro