This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C123G: DK-TM4C123G:

Part Number: DK-TM4C123G


hello ,

I was able to run  the program which were given in the tivaware examples  in DK-TM4C123GH6PGE . But while creating new project  for graphics example i am getting 


#1965 cannot open source file "drivers/cfal96x64x16.h" 

If you could provide the steps to execute or link the library . That will be helpfull

  • Hi,

      Please make sure you have the searthpath setup correctly so it can find the needed header files. When creating a new project, I will even suggest you first make a copy of an existing example project with a new project name. You will then add, remove, or modify any code you want. This may be easier. 

  • Hi Ganesh,
    I have not heard back from you. I assume the issue is resolved. I will close this thread for now. If you have new questions you can open a new thread or you can reopen this thread if you need further resistance.