Part Number: TM4C1294KCPDT
How can the CCP match edge events polarity be made to include trigger hysteresis or ability to set a threshold for edge trigger level? Point is a timer control event positive edge also triggers CCPn from a 3v3 valance level.
Seemingly a positive going edge should originate from ground to be counted as a valid CCPn positive edge. Otherwise pulses originate 3v3 pass just below logic high (VDD*0.65) shoot back up to VDD trigger an edge event.
Phantom edges can easily blend in with the expected CCPn positive edge events since the direction an edge originated is not being constrained by the CCPn hardware design. What is the point of setting a direction for edges polarity capture event if the edge direction is not being constrained by hardware?