Part Number: RM46L852
Other Parts Discussed in Thread: HALCOGEN
I have a quick question.
I want to communicate with a servo motor via 1.000.000 baud rate.
Reading the documentation of the motor it says it communicates at 1.000.000 baud rate with 0% tolerance.
Configuring SCI2 to 1.000.000 baud, results in 982143.
UART has tolerance of 3%.
Does this mean that even though my motor communicates with 1.000.000 baud, that if I use 982143 baud there will be no communication problems, information losses and similar?
Thanks,
David