Tool/software: TI-RTOS
Hello,
I am looking for any solution to detect the presence of the EPI SDRAM. I put the following code to a device where the RAM is not present and I can not upload any new code into the target. When I hit the debug the CCS says: Error connecting to the target
uint16_t * start = (uint16_t *)0x60000000;
uint16_t startVal = start[SDRAM_START_ADDRESS];
EK-TM4C12EXL TI 18.12.1.LTS RTOS 2.16.0.08 XDC: 2.32.0.06