Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Controller : TMS570LC4357
Tools using : CCS , HALCOGEN
Issue : Example given for TMS570LC43xx in HALCOGEN SCI over DMA is not working
Doing all the configuration as per given in the sample example file just i'm using the shared RAM area which I have configured properly in the .cmd file.
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Code used ///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
/* USER CODE END */
#include "HL_system.h"
#include "HL_sys_dma.h"
#include "HL_sci.h"
#include "stdio.h"
/* USER CODE END */
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
#define size 100
/* External connection (SCI3 TX -> SCI4 RX) is needed in case LOOPBACKMODE is defined as 0 */
#define LOOPBACKMODE 1
uint8 TX_DATA[size];
uint8 RX_DATA[size]={0xff};
#pragma SET_DATA_SECTION()
#if ((__little_endian__ == 1) || (__LITTLE_ENDIAN__ == 1))
#define SCI3_TX_ADDR ((uint32_t)(&(sciREG3->TD)))
#define SCI3_RX_ADDR ((uint32_t)(&(sciREG3->RD)))
#define SCI4_TX_ADDR ((uint32_t)(&(sciREG4->TD)))
#define SCI4_RX_ADDR ((uint32_t)(&(sciREG4->RD)))
#else
#define SCI3_TX_ADDR ((uint32_t)(&(sciREG3->TD)) + 3)
#define SCI3_RX_ADDR ((uint32_t)(&(sciREG3->RD)) + 3)
#define SCI4_TX_ADDR ((uint32_t)(&(sciREG4->TD)) + 3)
#define SCI4_RX_ADDR ((uint32_t)(&(sciREG4->RD)) + 3)
#endif
#define DMA_SCI3_RX DMA_REQ30
#define DMA_SCI4_TX DMA_REQ43
#define DMA_SCI4_RX DMA_REQ42
#define SCI_SET_RX_DMA (1<<17)
#define SCI_SET_RX_DMA_ALL (1<<18)
/* USER CODE END */
uint32 emacPhyAddress = 0U;
{
/* USER CODE BEGIN (3) */
uint32 sciTxData, sciRxData;
int i;
g_dmaCTRL g_dmaCTRLPKT1, g_dmaCTRLPKT2;
for (i=0; i<size; i++)
{
TX_DATA[i] = i;
}
sciInit();
/* Enable SCI loopback */
sciEnableLoopback(sciREG3, Digital_Lbk);
while (((sciREG3->FLR & SCI_TX_INT) == 0U) || ((sciREG3->FLR & 0x4) == 0x4))
{
} /* Wait */
dmaReqAssign(DMA_CH0, DMA_SCI3_TX);
dmaReqAssign(DMA_CH1, DMA_SCI3_RX);
sciRxData = SCI3_RX_ADDR;
while (((sciREG3->FLR & SCI_TX_INT) == 0U) || ((sciREG3->FLR & 0x4) == 0x4))
{
} /* Wait */
dmaReqAssign(DMA_CH0, DMA_SCI3_TX);
dmaReqAssign(DMA_CH1, DMA_SCI4_RX);
sciRxData = SCI4_RX_ADDR;
g_dmaCTRLPKT1.SADD = (uint32_t)TX_DATA; /* source address */
g_dmaCTRLPKT1.DADD = sciTxData; /* destination address */
g_dmaCTRLPKT1.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT1.FRCNT = size; /* frame count */
g_dmaCTRLPKT1.ELCNT = 1; /* element count */
g_dmaCTRLPKT1.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.PORTASGN = PORTA_READ_PORTB_WRITE;
g_dmaCTRLPKT1.RDSIZE = ACCESS_8_BIT; /* read size */
g_dmaCTRLPKT1.WRSIZE = ACCESS_8_BIT; /* write size */
g_dmaCTRLPKT1.TTYPE = FRAME_TRANSFER; /* transfer type */
g_dmaCTRLPKT1.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT1.ADDMODEWR = ADDR_FIXED; /* address mode write */
g_dmaCTRLPKT1.AUTOINIT = AUTOINIT_OFF; /* autoinit */
g_dmaCTRLPKT2.SADD = sciRxData; /* source address */
g_dmaCTRLPKT2.DADD = (uint32_t)RX_DATA; /* destination addr ss */
g_dmaCTRLPKT2.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT2.FRCNT = size; /* frame count */
g_dmaCTRLPKT2.ELCNT = 1; /* element count */
g_dmaCTRLPKT2.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.PORTASGN = PORTB_READ_PORTA_WRITE;
g_dmaCTRLPKT2.RDSIZE = ACCESS_8_BIT; /* read size */
g_dmaCTRLPKT2.WRSIZE = ACCESS_8_BIT; /* write size */
g_dmaCTRLPKT2.TTYPE = FRAME_TRANSFER; /* transfer type */
g_dmaCTRLPKT2.ADDMODERD = ADDR_FIXED; /* address mode read */
g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT2.AUTOINIT = AUTOINIT_OFF; /* autoinit */
dmaSetCtrlPacket (DMA_CH0, g_dmaCTRLPKT1);
dmaSetCtrlPacket (DMA_CH1, g_dmaCTRLPKT2);
dmaSetChEnable(DMA_CH0, DMA_HW);
dmaSetChEnable(DMA_CH1, DMA_HW);
dmaEnable();
/*Enable SCI3 Transmit and Receive DMA Request*/
sciREG3->SETINT |= SCI_SET_TX_DMA | SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
/*Enable SCI3 Transmit and SCI4 Receive DMA Request*/
sciREG3->SETINT |= SCI_SET_TX_DMA;
sciREG4->SETINT |= SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
#endif
{
if(RX_DATA[i] != TX_DATA[i])
{
break;
}
}
if(i<size)
{
printf("Fail\n");
}
else
{
printf("Pass\n");
}
while(1);
}
/* USER CODE END */
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// End of code ///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////