Other Parts Discussed in Thread: TLC2262, LM7705, TLV9062, TLV9002
Hi all:
Now it is necessary to make an industrial infrared non-contact temperature probe, and there are the following requirements for the devices used.Please recommend the mainstream chip
一、Please recommend a suitable MCU
16 or 32 bit microcontroller;Two-channel ADC, 16bit;1-way DA, 12bit;1-channel UART;flash, 32 KB;Etc.
二、Recommend suitable op/amp
Single power supply, high precision, low temperature drift, rail to rail, operational amplifier for industrial instruments, working normally at 3.3v.
三、Question: can TLC2262 have 0V output in single power mode?Or do you need dual power to output 0V?