This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello ti,
I am working on TMS470M06607 .
Currently we have TMS470M06607 usb stick , I am able to flash and execute the sample codes of TMS470M06607 using ccs and uniflash .
we developed a custom board with TMS470M06607 which is equivalent to TMS470M06607 usb mode, with a change removing usb format debug and replaced with JTAG for debugging .
so for flashing TMS470M006607 custom board ,we used a smartrf06 evaulation board JTAG pins to flash it , but we are unsuccessful .
link of evaluation board is .... http://www.ti.com/tool/SMARTRF06EBKb .
please help me to flash our board using smartrf06 evaulation board JTAG.
I have never used the XDS100v3 on a SMARTRF06EBKb . If the issue is using that hardware as an emulator, I will transfer this thread to that group. Did you create a target configuration for the XDS100v3 and the TMS470M06607? If you look at the "Advanced" tab of the target configuration file in Code Composer, it should look like this:
From that window you can test various parts of the scan chain by selecting a point on the chain and then clicking the "Test Connection" button. In the image above, the first level, IcePick, is selected.
That error message suggests a hardware problem. Do you have a diagram (or schematic) of the connections between the TMS470 and the SMARTRF06 board?