Part Number: RM46L852
Hello!
Quick question.
My application requires for Hercules to operate on battery.
Can you tell me where are the pins for +5V and GND for external power supply?
Also, what will happen if I do not remove the jumper that allows it to be powered via USB? Is it possible to leave that jumper on so I can flash new code while controller is being powered by external power supply or do I need to take the controller of source, then displace the jumper again, flash new code, and return the controller the way it was?
Thanks!
Marc