Part Number: TMS570LS0432
Other Parts Discussed in Thread: LAUNCHXL-TMS57004, TMDSEMU200-U, TMDSEMU110-U
Hi!
I'm using CCS v8.3.0, and Windows 10 (x64)...
I've been working with the TMS570LS04 (Hercules Launchpad) for about a month, and recently I plugged it in and the module can't connect. I didn't do anything in particular to brick the module (that I know of)...
I last remember, I flashed it, saw my code worked in the debugger, and then unplugged the module. I returned to it the next day and couldn't connect (getting that 'SC_ERR_FTDI_OPEN' error). A windows 10 pop-up would gives the "USB device not recognized" pop-up every time I plug it in; also, I've tried uninstalling and reinstalling CCS/the hercules drivers, and am unable to see XDS100v2 in Window's control panel. I've even tried a different USB cable.
The SCI1RX and SCI1TX LEDs (D5 & D6) are dim, and stay dimly lit as long as power is supplied to the module (in my case, through the micro-usb to my computer). D1 is the only LED on all the way.The ERR LED (D10) flashes on reset. I've tried using the xdsdfu utility in "..\ccsv8\ccs_base\common\uscif\xds110"; however, I'm unable to recover the device. I checked the voltages on the 5V & 3.3V pins, and they're at the correct voltages. In fact, my application still runs fine... I have the controller outputting CAN messages, and it looks like the program is acting just as it had last I was able to flash the controller.
I'm unsure how to proceed with debugging this issue. Any help is greatly appreciated!
Thanks,
John Lodi