Part Number: TM4C129XNCZAD
Device: TM4C129XNCZAD
Driverlib: 2.1.4.178
Predefined Compiler Symbols:
PART_TM4C129XNCZAD
TARGET_IS_TM4C129_RA2
DEBUG
When initialising the PWM using...
PWMClockSet( PWM0_BASE, PWM_SYSCLK_DIV_1 );
The ASSERT at the entry of this function does not include PWM_SYSCLK_DIV_1 in the validation checks for the second parameter, and consequently the ASSERT triggers.
Is this an oversight? Or is PWM_SYSCLK_DIV_1 actually an illegal parameter?
Regards.