Hello team,
For the newly released MCAL below are the violations for the AUTOSAR standards.
MCAL version: AUTOSAR_MCAL_TMS570LSx-05.40.00-
[Error] A205 - Parameter 'Mcu/McuGeneralConfiguration/McuEWait' uses implementation config variant 'VARIANT_PRE_COMPILE' | but this variant is not contained in supported config variants of module. [Mcu_definition_bswmd.arxml] |
[Error] A204 - Line: 13 - The 'autosar.org/.../r4.0:DEFAULT-VALUE' element is invalid - The value '144QFP' is invalid according to its datatype 'autosar.org/.../r4.0:IDENTIFIER' - The Pattern constraint failed. [Port_definition_bswmd.arxml] | |
[Error] A204 - Line: 13 - The 'autosar.org/.../r4.0:SHORT-NAME' element is invalid - The value '144QFP' is invalid according to its datatype 'autosar.org/.../r4.0:IDENTIFIER' - The Pattern constraint failed. [Port_definition_bswmd.arxml] | |
[Error] A204 - Line: 13 - The 'autosar.org/.../r4.0:SHORT-NAME' element is invalid - The value '337BGA' is invalid according to its datatype 'autosar.org/.../r4.0:IDENTIFIER' - The Pattern constraint failed. [Port_definition_bswmd.arxml] | |
[Error] A207 - Minimum value of parameter 'Port/PortConfigSet/PortContainer/PortPin/PortPinId' in VSMD (0) may not be smaller than minimum value defined in StMD (1). [Port_definition_bswmd.arxml] | |
[Error] A221 - SHORT-NAME '144QFP' is not valid. [Port_definition_bswmd.arxml] | |
[Error] A221 - SHORT-NAME '337BGA' is not valid. [Port_definition_bswmd.arxml] |
Thanks
Kishore