Part Number: TM4C1294KCPDT
Tool/software: TI C/C++ Compiler
Hi All,
TM4C1294KCPDT - Serial - CDC example.
I have create an application that runs on top of USB CDC layer. (i.e. application that uses CDC layer as a channel).
This is working fine.
I wish to change the USB speed to 2.0 from existing 1.1.
In order to achieve this the following change is made,
In usbdcdc.c, structure g_pui8CDCSerDeviceDescriptor is modified with the 3rd parameter, i.e from USBShort(0x110) to USBShort(0x0200). and usblib project is rebuild and then the application project usbserialdevice_EK_TM4C1294XL_TI is rebuild. And then the application is executed.
Is the above procedure correct? Or is there any other settings to be done from the application?
Thanks,
Jay