Part Number: TM4C123GH6PM
I am trying to read configure ADC module in TM4C123GH6PM Evaluation board. I want to read voltage at pin PE3. But my code is not working. Please help as I am new to embedded. I am following TM4C123GH6PM workshop.
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
int main(void)
{
uint32_t result[1];
volatile uint32_t x;
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinTypeADC(GPIO_PORTE_BASE,GPIO_PIN_3);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE,3,0,ADC_CTL_CH0);
ADCSequenceEnable(ADC0_BASE, 3);
while(1)
{
ADCIntClear(ADC0_BASE, 3);
ADCProcessorTrigger(ADC0_BASE, 3);
while(!ADCIntStatus(ADC0_BASE, 3, false))
{
}
ADCSequenceDataGet(ADC0_BASE, 3, result);
x = result[0];
}
}