Other Parts Discussed in Thread: TIDA-010010
Dear Sir / Madam,
We have a requirement for Evaluation board for IIOT Applications-CNC Machine with industrial standards and it should have the following minimum feature.
1. Ethernet
2. Wi-Fi
3. USB Ports- 2 No's.
4. Micro SD Card Slot.
5. RS 485 or compatible pins.
6. UART/RS232
7. SPI
8. Analog Input Pins- 12 Pins for Sensors(Vibration,Temperature,CT/PT,etc).
9. GPIO Pins- 8 Pins.
Kindly Suggest the suitable and efficient board for the same.
Thanking you.
Regards,
Naveen K