Part Number: TM4C1231H6PM
Hello,
The RTC of TM4C1231 can't be saved When power up again during we test board function . About 30% failure rate for this. Would you please give your advice on this? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1231H6PM
Hello,
The RTC of TM4C1231 can't be saved When power up again during we test board function . About 30% failure rate for this. Would you please give your advice on this? thanks.
Hi Bob,
Thanks for your support.
System time can't be saved after several power on and down. So we suspect that the RTC can't work well.
We tested the PIN 37 which the impedance reduce to 100Ω, but the good chip is about 1MΩ to this PIN.
We also do the SWAP A-B, B-A, Fault Phenomenon Following Chip TM4C1231 .
Hi Bob,
After we installed a 3.3V battery on the circuit board, then the voltage of battery was pulled down to about 1V. The resistance of pin 37(VABT) reduce to about 100Ω.
Now we are applying the FA to verify this issue. thanks.