This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM: Connection to DH22

Part Number: TM4C123GH6PM

HI

I am trying to communicate with the DH22 sensor using CCS and tiva launchpad. I am unable to get any signal from the dh22 

I have given required delay for the communication so that the sensor can read but the output of the sensor is always high during the initial procedure and does not provide the data to the microcontroller.

Only thing i am confused about is the 2 s delay is on power up means the delay after issuing the start signal from the cpu or on connectin therm to the voltage levels.