Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS0914: Cannot enable MIBSPI1 chip select #3 in HALCoGen

Part Number: TMS570LS0914
Other Parts Discussed in Thread: HALCOGEN,

Tool/software: Code Composer Studio

Hi, I'm having difficulty enabling the chip select #3 for the MIBSPI1 module of the TMS570LS0914 (PZ, 100 pins) in HALCoGen. In HALCoGen, I've enabled MIBSPI1 driver, then went to MIBSPI1->MIBSPI1 Port. I can't select SPI mode for the SCS[3] pin mode. The checkbox is grayed out and only the GIO is selected. Then, if I sent to a group using this chip select, the CS doesn't get pulled-down when I probe using a logic analyzer. Any idea how to fix this? Thanks.

  • While HALCoGen wasn't able to select SPI mode for the chip select #3. I was able to modify SCS[3] manually in the generated code in the register mibSPIREG1->PC0. The chip select is now pulled-down when I probe using the logic analyzer. Any idea why HALCoGen doesn't allow this modification?
  • Thank you for pointing this out. I will check with SW team. CS[3] is available on pin 39 of LS0914 device, and this pin is muxed with NHET1[21]. The Pinmux on HALCoGen doesn't list pin 39.