Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: UNIFLASH, EK-TM4C123GXL
Hi, I have an application done on Keil uVision for a Tiva TMC4123G launchpad. I would like to upload the program to a custom board using a TM4C123GH6PM. I found this datasheet http://www.ti.com/lit/an/spma075/spma075.pdf "UsingTM4C12xDevicesOverJTAGInterface" pg. 15. My question is it possible to upload the program using Keil or I should use Code Composer instead? Another question I have is about the external 16MHz
since I'm using the internal clock PIOSC in my program then I could leave the MOSC pins floating correct? I also found a reference design that shows how to properly add pull up resistors for some of the JTAG pins.
https://e2e.ti.com/support/microcontrollers/other/f/908/t/325440?custom-board-jtag-programming . Last question is if I place back the 1x2 header between pins H24 and H25 I can still use the main MCU from the launchpad once I'm done uploading the program to the custom board correct? I know my questions are silly but I would greatly appreciate any suggestions and if there any extra recommendations I should follow to upload my program to the custom board. Thanks.