Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: MAX232, HDC1010,
Hello,
I'm not able to interface SIM900 Gsm module with the tiva C series TM4C123GXL launchpad.
Can I get help with the code and connections Also do I need MAX232 for interfacing.
How can I use HDC1010 for real time humidity detection.Also is it possible to connect this module independently,since I'm want to sense the humidity of the soil.But there is just one USB port available in the module which makes connection with a TM4C123GH6PM difficult.