Hello all:
I am designing a sound FX processor for my senior project, and would like to do my debug and DSP flashing via JTAG. My question is this; since I plan to use the XDS110 probe, how much circuitry do I need on the board itself? I know that there should be pull up and pull-down resistors on some of the JTAG pins, but are those integrated into the JTAG control probe, or am I responsible for designing those elements into my circuit? If i add them and it turns out I don't need them, I foresee issues with signal integrity.
Any input would be appreciated!