This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1290NCPDT: SPI interface pin function

Part Number: TM4C1290NCPDT

Hi,

I am interfacing Standard x1 SPI flash to the SSI interface of the TM4C1290.

As per datasheet TM4C1290 supports Bi and Quad SSI interfaces only.

Can it is possible to interface Standard SPI peripheral with the TM4C1290 ?

If it is possible , then which are MISO and MOSI lines in SSI0XDAT0 & SSI0XDAT1 ?

Thanks & regards,

Divya