This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPTM Edge count/Time capture modes

Guru 56418 points

Part Number: TM4C1294KCPDT

Seemingly datasheet makes an incorrect statement that edge count (capture) mode starts when enable bit is set. I noticed this issue some time ago and added Tivaware capture bit set define TnMR in the timer configuration. However the same section omits any comment of TnCMR bit must be cleared even though POR defaults 0x0, Tivaware define sets TnCMR (0x00000004) anyone adds that to HWREG call will not get the intended resutls. Datasheet subject order has edge count prior to edge time mode. Yet define (TIMER_TAMR_TACMR) defaults timer for edge time mode. 

That issue is not obvious by reading datasheet GPTM analysis. Tivaware omits distinction (hw_timer.h) defines to properly set the two capture modes for Edge or Time via TnCBR bits in the GPTMTnMR register. The GPTMCFG register does not set EDGE capture mode default, a foot note bottom of GPTMTnMR states the mode is set in GPTMCFG. Yet GPTMCFG only sets the timer spilt points and has no affiliation how GPTMTnMR bits default 0x0 reserved.

The entire subject of CCP capture mode could easily be rectified by adding a separate define for each mode (Edge/Time) as it relates to HWREG calls to symbolically set register bits.

13.3.3.3 Input Edge-Count Mode

In Edge-Count mode, the timer is configured as a 24-bit up- or down-counter including the optional prescaler with the upper count value stored in the GPTM Timer n Prescale (GPTMTnPR) register and the lower bits in the GPTMTnR register. In this mode, the timer is capable of capturing three types of events: rising edge, falling edge, or both. To place the timer in Edge-Count mode, the TnCMR bit of the GPTMTnMR register must be cleared. The type of edge that the timer counts is determined by the TnEVENT fields of the GPTMCTL register. During initialization in down-count mode, the GPTMTnMATCHR and GPTMTnPMR registers are configured so that the difference between the value in the GPTMTnILR and GPTMTnPR registers and the GPTMTnMATCHR and GPTMTnPMR registers equals the number of edge events that must be counted. In up-count mode, the timer counts from 0x0 to the value in the GPTMTnMATCHR and GPTMTnPMR registers.

Note that when executing an up-count, that the value of GPTMTnPR and GPTMTnILR must be greater than the value of GPTMTnPMR and GPTMTnMATCHR. Table 13-7 on page 961 shows the values
that are loaded into the timer registers when the timer is enabled.

When software writes the TnEN bit in the GPTM Control (GPTMCTL) register, the timer is enabled for event capture.

GPTMTnMR REG2, REG3:

1:0 TnMR RW 0x0 GPTM Timer B Mode
The TnMR values are defined as follows:
Value Description
0x0 Reserved
0x1 One-Shot Timer mode
0x2 Periodic Timer mode
0x3 Capture mode

2 GPTM Timer B Capture Mode
The TnCMR values are defined as follows:
Value Description
0 Edge-Count mode
1 Edge-Time mode

#define TIMER_TAMR_TACMR        0x00000004  // GPTM Timer A Capture Mode (0x00000000)
#define TIMER_TAMR_TAMR_M       0x00000003  // GPTM Timer A Mode
#define TIMER_TAMR_TAMR_1_SHOT  0x00000001  // One-Shot Timer mode
#define TIMER_TAMR_TAMR_PERIOD  0x00000002  // Periodic Timer mode
#define TIMER_TAMR_TAMR_CAP     0x00000003  // Capture mode

#define TIMER_TBMR_TBCMR        0x00000004  // GPTM Timer B Capture Mode (0x00000000)
#define TIMER_TBMR_TBMR_M       0x00000003  // GPTM Timer B Mode
#define TIMER_TBMR_TBMR_1_SHOT  0x00000001  // One-Shot Timer mode
#define TIMER_TBMR_TBMR_PERIOD  0x00000002  // Periodic Timer mode
#define TIMER_TBMR_TBMR_CAP     0x00000003  // Capture mode

  • Hi BP101,

    BP101 said:
    When software writes the TnEN bit in the GPTM Control (GPTMCTL) register, the timer is enabled for event capture.

    I don't really see a problem with this statement. It merely says that GPTM timer module is enabled and is ready for event capture after TnEN bit is set. Certainty there are other configurations that also need to take place too. For example, you will need to select between edge-time or edge-count mode by programming the TNCMR bit with 0 selecting the edge-count mode and 1 selecting the edge-time mode. You can certainly be picky about the wording but personally it is clear to me that you must also program the TnCMR bit to 0 to select edge-count mode. 

     I wonder why you don't use the TivaWare API TimerConfigure with the TIMER_CFG_A_CAP_COUNT. This would have configured the timer for edge_count mode properly. As far as the #define TIMER_TBMR_TBCMR, this define is not even used by any driverlib API. I agree that it could have added another #define to distinguish between the edge-time or edge_count for someone who wants to use these macros.