Part Number: TMS570LC4357
Hello,
I want to access L2RAMW area with R/W 64-bit access size.
I propose to write the following code :
uint64 READ_64BIT_DATA(uint64* startAddr)
{
uint64 READ_VALUE;
READ_VALUE = (uint64)(*startAddr);
return(READ_VALUE);
}
Is that the good way to access in 64-bit size to the memory ? How to be sure that this code will not generate a 2x32-bit access to memory ?
Thanks for your answer.
François