Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
I am new to TI microcontrollers and HALCoGen. I am using the TMS570LC43HDK evaluation board.
I understand that LIN2/SCI2 is connected to the XDS to provide UART functionality etc.
I want to use LIN1/SCI1 as SCI and have a second UART and having trouble understanding how to configure HALCoGen and actually use it on the board.
To do this:
a. I enable SCI1 driver in the Driver Enable tab of HALCoGen
b. I go to PinMux tab. There is LIN2/SCI2 but no LIN1/SCI1 there!
c. I also see on P4, LIN2RX being muxed with N2HET2[19] and on T5, LIN2TX beign muxed with N2HET2[20].
d. I do see a SCI1 tab available. On that tab I see SCI1 is SCI MODE CONFIGURATION OF LIN1 MODULE. API'S ARE PLACED IN SCI.C
e. Shouldn't I expect LIN1/SCI1 to be similar to LIN2/SCI2? Why is that option missing in the Pin Muxing tab?
f. In the schematic for the HDK, I see B7/LINTX and A7/LINRX coming out both as USB_LINTX/USB_LINRX (refer to page 23) as well as LIN_TX/LIN_RX (refer to page 29 for the J11 header).
The SCI3/SCI4 configuration seems to be OK in HALCoGen and I can understand how they are brought out to J11 also (from the schematic).
I want to understand how to use SCI1 on the TMS570LC43 HDK.
I appreciate any insight you can provide on this issue.
Thank you
Subu