Hello,
I am using the unsigned USB drivers provided with the TI-RTOS USB Serial DFU project, see code below.
The files enumerate two devices, a runtime usb dfu device and a cdc serial device.
I have tried to find out if the drivers run in kernel or user mode.
If I am not mistaken, when a .sys file is used, as is the case (WinUSB.sys and usbser.sys), they run in kernel mode.
On the other hand, the driver description says
[...] All this file does, therefore, is ensure that the DFU drivers and WinUSB subsystem are installed to support switching from DFU runtime mode into "real" DFU mode in preparation for download and upload operations.
Since I need to purchase a certificate to be able to sign the drivers for Windows 10, I need to know if I need to purchase an extended validation certificate (kernel and user mode) or if just a regular certificate (only user mode) will do.
I tried finding answers on the Windows Hardware Dev Center but it left me quite confused.
Can anyone help me out for these drivers specifically or better yet, how to identify if a driver runs in kernel or user mode when only the .inf file is available? It is greatly appreciated.
Full unmodified driver files for reference:
; ----------------------------------------------------------------------------- ; ; TivaWare USB DFU Runtime device driver installer ; ; The composite devices supported by this INF file contains a HID mouse with ; a Device Firmware Upgrade runtime interface (basically, just a stub that ; tells the host that the device supports DFU). Since HID is supported ; natively by Windows, no HID-specific sections are required here. All this ; file does, therefore, is ensure that the DFU drivers and WinUSB subsystem ; are installed to support switching from DFU runtime mode into "real" DFU ; mode in preparation for download and upload operations. ; ; This device offers DFU on interface number 1 and publishes PID 0x0A while in ; runtime mode. When it is switched to DFU mode (implemented by the boot_usb ; boot loader), the device reenumerates and publishes PID 0xFF instead. This ; is seen as a different device by Windows and requires a second INF file to ; support it. This INF file is boot_usb.inf which installs exactly the same ; files as this one. ; ; ----------------------------------------------------------------------------- ; NOTE: When you customize this INF for your own device, create a new class ; name (Class) and a new GUID (ClassGuid). GUIDs may be created using the ; guidgen tool from Windows Visual Studio or the Windows SDK. [Version] Signature = "$Windows NT$" Class = USBLibDFURuntimeDeviceClass ClassGuid={0D42186B-31A8-4800-B875-1A5525A407B9} Provider = %MFGNAME% DriverVer=12/15/2015,2.1.1.71 ; ========== Manufacturer/Models sections =========== [Manufacturer] %MFGNAME%=USBLibDFUDevice_WinUSB,NTx86,NTamd64 ; NOTE: Replace the VID and PID in the following two sections with the ; correct values for your device. [USBLibDFUDevice_WinUSB.NTx86] %DESCRIPTION%=DFU_Install,USB\VID_1CBE&PID_0102&MI_02 [USBLibDFUDevice_WinUSB.NTamd64] %DESCRIPTION%=DFU_Install,USB\VID_1CBE&PID_0102&MI_02 ; =================== Installation =================== [ClassInstall32] AddReg=AddReg_ClassInstall [AddReg_ClassInstall] HKR,,,,"%DeviceClassDisplayName%" HKR,,Icon,,-1 [DFU_Install.NTx86] Include=winusb.inf Needs=WINUSB.NT CopyFiles=System32_CopyFiles [DFU_Install.NTamd64] Include=winusb.inf Needs=WINUSB.NT CopyFiles=SysWOW64_CopyFiles CopyFiles=System64_CopyFiles [DFU_Install.NTx86.Services] Include=winusb.inf AddService=WinUSB,0x00000002,WinUSB_ServiceInstall [DFU_Install.NTamd64.Services] Include=winusb.inf AddService=WinUSB,0x00000002,WinUSB_ServiceInstall [WinUSB_ServiceInstall] DisplayName = %WinUSB_SvcDesc% ServiceType = 1 StartType = 3 ErrorControl = 1 ServiceBinary = %12%\WinUSB.sys [DFU_Install.NTx86.Wdf] KmdfService=WINUSB, WinDFU_Install [DFU_Install.NTamd64.Wdf] KmdfService=WINUSB, WinDFU_Install [WinDFU_Install] KmdfLibraryVersion=1.9 [DFU_Install.NTx86.HW] AddReg=Dev_AddReg [DFU_Install.NTamd64.HW] AddReg=Dev_AddReg ; NOTE: The following GUID is used by software that accesses USBLib DFU ; devices (dfuprog and LM Flash Programmer). If you want your device to be ; accessible by these tools, do not change it. [Dev_AddReg] HKR,,DeviceInterfaceGUIDs,0x10000,"{D17C772B-AF45-4041-9979-AAFE96BF6398}" [DFU_Install.NTx86.CoInstallers] AddReg=CoInstallers_AddReg CopyFiles=CoInstallers_CopyFiles [DFU_Install.NTamd64.CoInstallers] AddReg=CoInstallers_AddReg CopyFiles=CoInstallers_CopyFiles [CoInstallers_AddReg] HKR,,CoInstallers32,0x00010000,"WdfCoInstaller01009.dll,WdfCoInstaller","WinUSBCoInstaller2.dll" [CoInstallers_CopyFiles] WinUSBCoInstaller2.dll WdfCoInstaller01009.dll [System32_CopyFiles] lmusbdll.dll lmusbdll.lib lmdfu.dll lmdfu.lib [System64_CopyFiles] lmusbdll.dll, lmusbdll64.dll lmusbdll.lib, lmusbdll64.lib lmdfu.dll, lmdfu64.dll lmdfu.lib, lmdfu64.lib [SysWOW64_CopyFiles] lmusbdll.dll lmusbdll.lib lmdfu.dll lmdfu.lib [DestinationDirs] CoInstallers_CopyFiles=11 System32_CopyFiles=10,system32 SysWOW64_CopyFiles=10,syswow64 System64_CopyFiles=10,system32 ; ================= Source Media Section ===================== [SourceDisksNames] 1 = %DISK_NAME%,,,\i386 2 = %DISK_NAME%,,,\amd64 [SourceDisksFiles.x86] WinUSBCoInstaller2.dll=1 WdfCoInstaller01009.dll=1 lmusbdll.dll=1 lmusbdll.lib=1 lmdfu.dll=1 lmdfu.lib=1 [SourceDisksFiles.amd64] WinUSBCoInstaller2.dll=2 WdfCoInstaller01009.dll=2 lmusbdll.dll=1 lmusbdll.lib=1 lmdfu.dll=1 lmdfu.lib=1 lmusbdll64.dll=2 lmusbdll64.lib=2 lmdfu64.dll=2 lmdfu64.lib=2 ; =================== Strings =================== ; Note: Replace these as appropriate to describe your device. [Strings] MFGNAME="Texas Instruments Inc." DESCRIPTION="TivaWare Device Firmware Upgrade (runtime mode)" WinUSB_SvcDesc="WinUSB" DISK_NAME="TivaWare Install Disk" DeviceClassDisplayName="TivaWare Device Firmware Upgrade (runtime mode)"
; ; TivaWare USB CDC (serial) driver installation file. ; [Version] Signature="$Windows NT$" Class=Ports ClassGuid={4D36E978-E325-11CE-BFC1-08002BE10318} Provider=%MFGNAME% LayoutFile=layout.inf DriverVer=12/14/2015,2.1.1.71 [Manufacturer] %MFGNAME%=VirComDevice,NT,NTamd64 [DestinationDirs] DefaultDestDir = 12 [VirComDevice.NT] %DESCRIPTION%=DriverInstall,USB\VID_1CBE&PID_0102&MI_00 [VirComDevice.NTamd64] %DESCRIPTION%=DriverInstall,USB\VID_1CBE&PID_0102&MI_00 [DriverInstall.NT] Include=mdmcpq.inf CopyFiles=FakeModemCopyFileSection AddReg=DriverInstall.NT.AddReg [DriverInstall.NT.AddReg] HKR,,DevLoader,,*ntkern HKR,,NTMPDriver,,usbser.sys HKR,,EnumPropPages32,,"MsPorts.dll,SerialPortPropPageProvider" [DriverInstall.NT.Services] AddService=usbser, 0x00000002, DriverServiceInst [DriverServiceInst] DisplayName=%SERVICE% ServiceType=1 StartType=3 ErrorControl=1 ServiceBinary=%12%\usbser.sys [Strings] MFGNAME = "Texas Instruments, Inc." DESCRIPTION = "TivaWare USB serial port with DFU" SERVICE = "TivaWare USB CDC serial port"