Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129XNCZAD: Encryption chip speed, ULPI throughput and SD card readwrite speed

Part Number: TM4C129XNCZAD
Other Parts Discussed in Thread: AM5706

Hello TI!

From what I've gathered about the components offered by TI:

TUSB1002ARGET: Is a USB 3.0 interface chip

TM4C129XNCZAD: Is a high speed processing unit

SN74AVCA406L: Is a microSD card interfacing chip

The project we're working on is to develop a USB3.0 (target 800/480 Mbps read/write) encrypted, microSD card storage device. This brings up a few issues, but my understanding is that the USB3.0 interface chip (TUSB1002ARGET) can handle the dataspeed required, this can connect to the processing unit (TM4C129XNCZAD) via ULPI which can encrypt the data which is passed onto the microSDcard interface (SN74AVCA406L).

How fast is: SN74AVCA406L? Can it handle 800/480Mbps? Can the processing unit handle the desired encryption speed and is it capable of handling the format of the SD card files?

My main confusion when going through the documentation is the actual throughput of components...

Regards!

Fujimi