Part Number: TM4C123GE6PM
Hello,
I'm using TI hardware to design a USB device. I have a software application on the host (PC) that connects and communicates to it. If I have two devices plugged in with the same VID,PID but unique SNs can I fgure out of there is an open connection to a device already? I'm trying to prevent my software host app from connecting to the same device twice - I'd like to force the user to select a different device if the current device already has a connection (pipe I think) to the software application.