This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294KCPDT: Systick speed NVIC clock source

Guru 56418 points

Part Number: TM4C1294KCPDT

Anybody even realize Systick clock source defaults PIOSC/4 (250ns tick)? 

Why is there no Tivaware configuration for REG1 {CLK_SRC bit [2]} inside (systick.c)? It seems a reasonable deduction Systick resides inside NVIC, it too clocks PIOSC/4 (4MHz), 250ns tick rate to handle Application interrupt requests from the CPU. The main clock tree Fig 5-5 indicates SYSCLK feeds CPU (Fig 2-1) and no indication NVIC may be using PIOSC/4 (4Mhz) for Systick clock source.

The Systick reload period we often set for the interrupt handler most would assume F=1/p SYSCLK speed is 100x slower then expected. So if you thought Systick reload period you had set for 5ms interrupts it is actually 150ms based on PIOSC &! SYSCLK. 

There is no indication Figure 2-1 NVIC even sources SYSCLK, is anyone aware PIOSC/4 may be the default clock source for NVIC too? Why would NVIC not use the same PIOSC/4 clock source as the default imbedded timer Systick?

The fact that Systick concatenated edge times and GPTM edge times mode TnV, TnR registers results are so sporadic perhaps a similar issue? Seemingly NVIC clock source PIOSC/4 interrupt vector handlers swagger due to application speed MSP stacking at SYSCLK speeds. Handler swagger may not be detectable until a very slow GPIO/CCP edge time source challenges NVIC to maintain Synchronous with PLL derived SYSCLK relative to application and CPU instruction decode.

  • Who ever knew Systick clock source defaulted  PIOSC/4 or 4Mhz?

     /* Set PIOSC clock source to use SYSCLK */
     HWREG(NVIC_ST_CTRL) |= NVIC_ST_CTRL_CLK_SRC;

  • You are correct that the default value of the SysTick clock source is PIOSC/4. However, the TivaWare function SysTickEnable() sets the clock source to system clock as it enables the SysTick interrupt. The rest of the NVIC is always clocked the system clock, the same clock that clocks the CPU.
  • Bob Crosby said:
    TivaWare function SysTickEnable()

    Sort of a conundrum all other TM4C1294 peripheral enable calls do not force change a peripherals source clock rate without designer knowing. Not even a bread crumb clue main clock tree figure PIOSC even enters NVIC. Had no idea PIOSC was even entered ARM Core and a bit upset clocking inputs are for most part not illustrated in most peripheral blocks.