Part Number: TMS570LS0432
Other Parts Discussed in Thread: CODECOMPOSER
Tool/software: Code Composer Studio
I am writing a bootloader for my project. I have two projects in my workspace, boot_uart and IR4. I have edited the .cmd files for both projects so that the bootloader loads FLASH0 at 0x00001500 and IR4 loads in FLASH1 beginning at address 0x00020000.
In CodeComposer Studio I can load and run the bootloader or I can load and run IR4. They load to the expected flash memory location. The problem is that the other project space gets erased when I load a project. i.e. when I load the bootloader FLASH1 is erased and is all 0xFFFFFFFF. Likewise if I load IR4 the FLASH0 space is erased and is all 0xFFFFFFFF.
How can I load both projects concurrently to their respective flash memory space?
When I did this on an STM32F429 there was a Bind utility that would create a single image from the two programs. I have not been able to find an equivalent for the Hercules.
here are my .cmd files:
Bootloader: bl_link.cmd:
--retain="*(.intvecs)"
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH_API (RX) : origin=0x00000020 length=0x000014E0
FLASH0 (RX) : origin=0x00001500 length=0x0001EB00 //LS04x and RM42 Flash size is 0x60000
FLASH1 (RX) : origin=0x00020000 length=0x0003CB00 //LS04x and RM42 Flash size is 0x60000
SRAM (RW) : origin=0x08002000 length=0x00006000 //LS04x and RM42 SRAM size is 0x8000
STACK (RW) : origin=0x08000000 length=0x00002000
}
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI :
{
..\Debug\Fapi_UserDefinedFunctions.obj (.text)
..\Debug\bl_flash.obj (.text)
--library= F021_API_CortexR4_BE.lib < FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.SetActiveBank.obj
FlashStateMachine.InitializeFlashBanks.obj
FlashStateMachine.EnableMainSectors.obj
FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.ScaleFclk.obj
Init.obj
Utilities.CalculateEcc.obj
Utilities.WaitDelay.obj
Utilities.CalculateFletcher.obj
Read.MarginByByte.obj
Read.Common.obj
Read.FlushPipeline.obj
Read.WdService.obj
Async.WithAddress.obj
Program.obj > (.text)
} load = FLASH_API, run = SRAM, LOAD_START(api_load), RUN_START(api_run), SIZE(api_size)
.text > FLASH0
.const > FLASH0
.cinit > FLASH0
.pinit > FLASH0
.data > SRAM
.bss > SRAM
}
IR4: sys_link.cmd:
/*----------------------------------------------------------------------------*/
/* sys_link_freeRTOS.cmd */
/* */
/*
* Copyright (C) 2009-2016 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Linker Settings */
--retain="*(.intvecs)"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
KERNEL (RX) : origin=0x00020020 length=0x00008000
FLASHCRC(RW) : origin=0x00028020 length=0x00000040
FLASH0 (RX) : origin=0x00001500 length=0x0001EB00 //LS04x and RM42 Flash size is 0x60000
FLASH1 (RX) : origin=0x00028060 length=0x00037FA0
STACKS (RW) : origin=0x08000000 length=0x00000800
KRAM (RW) : origin=0x08000800 length=0x00000800
RAM (RW) : origin=(0x08000800+0x00000800) length=(0x00007800 - 0x00000800)
/* USER CODE BEGIN (2) */
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
/* FreeRTOS Kernel in protected region of Flash */
.kernelTEXT : {} > KERNEL
.cinit : {} > KERNEL
.pinit : {} > KERNEL
/* Rest of code to user mode flash region */
.text : {} > FLASH1
.const : {} > FLASH1
/* FreeRTOS Kernel data in protected region of RAM */
.kernelBSS : {} > KRAM
.kernelHEAP : {} > RAM
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
FEE_TEXT_SECTION : {} > FLASH1
FEE_CONST_SECTION : {} > FLASH1
FEE_DATA_SECTION : {} > RAM
/* USER CODE BEGIN (4) */
.section_to_be_verified_code: { *(.text) } > FLASH1, palign=8, fill=0xffffffff, crc_table(link_crc_table_name, algorithm = TMS570_CRC64_ISO)
.section_to_be_verified_consts: { *(.const) } > FLASH1, palign=8, fill=0xffffffff, crc_table(link_crc_table_name, algorithm = TMS570_CRC64_ISO)
.TI.crctab: > FLASHCRC palign=8
/* USER CODE END */
}
/* USER CODE BEGIN (5) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Misc */
/* USER CODE BEGIN (6) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
Your assistance is appreciated.
ken