This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: EK-TM4C123GXL: Cannot install Tiva Ware drivers in Windows 10

Hello sir,

I have the same issue.Just downloaded SW-TM4C-2.1.4.178 and when Im trying to install, the setup wizard is not responding. My OS is w10.

  • Hello Fatich,

    As in the whole .exe file won't run properly to install TivaWare?? Can you post screenshots? Also can you try and run it as an Administrator? Lastly, is there any company restrictions on running software on your machine?

    I've not heard of the TivaWare installer not working so I suspect something either from Windows or from a firewall/anti-virus standpoint is interfering with it.
  • Hello Fatich,

    I haven't heard back from you, so I’m assuming you were able to resolve your issue.

    I will close this thread now, but if you have not solved this issue then post a reply below (or open a new thread if the thread has locked due to time-out).