Hello,
I have a question regarding silicon erratum FTU#08 (FlexRay Transfer Unit Not Disabled On Memory Protection Violation (MPV) Error - SPNZ232B). In the event that a memory protection violation occurs and the FTU does not get disabled, and none of the suggested workarounds are implemented (so FTU stays enabled), does memory protection still successfully prevent the out-of-bounds write? Or is the FTU able to write to out-of-bounds memory despite the memory protection restrictions?
Thanks for the help.