Part Number: SW-EK-TM4C123GXL
Other Parts Discussed in Thread: LM35, EK-TM4C123GXL, TM4C123GH6PM
Tool/software: Code Composer Studio
Hello !
I am trying to interface a temperture sensor(LM35) with the Tiva Launchpad(EK-TM4C123GXL).
In order to do so, I modified a source code taken from an example. I configured the PE_3 pin as an ADC input pin.
But at the same time, I went through the Driver Peripheral Library for tm4c123gh6pm and saw an example for using the GPIO pins as an input pin.
So, accordingly, I modified my code and configured PE_2 as an input pin.
Both the configurations were made in the same code so that I could understand the difference between them.
But I am unable to do so, can you please tell me which of the either configurations would take in the output of the LM35 sensor, send it to the ADC and give me the corresponding values.
//Header Files needed to access the TIVA APIs
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/adc.h" //contains definitions for the ADC driver
int main(void)
{
//Var for the input GPIO
int32_t i32Val;
//Using Sequencer 1 of FIFO size = 4, hence creating an array to store its data
uint32_t ui32ADC0Value[4];
// var for storing the average of the temperature.
volatile uint32_t ui32TempAvg; //volatile makes them un-optimizable for the compiler
volatile uint32_t ui32TempValueC;
volatile uint32_t ui32TempValueF;
//Set up the system clock again to run at 40MHz
/* # PLL runs on 400 MHz
* -- this frequency is divided by 2 by default
* -- additional dividing factors between 5 & 25 can be used
* -- Here we use 5 (a total of 2+5=10)
* -Use PLL
* -Use main OSC as the system clock
* -Run it at 16 MHz
*/
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
//Enable the ADC0
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
//Enable the PE3 to be an input pin
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); //Enables the clock to PORT E
// Wait for the GPIOA module to be ready.
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOA))
{}
//Register the port level interrupt handler for all the pin interrupts
//GPIOIntRegister(GPIO_PORTE_BASE, PortEIntHandler);
/* PE_2 : INPUT PIN
* PE_3 : ADC INPUT PIN
*/
GPIOPinTypeGPIOInput(GPIO_PORTE_BASE,GPIO_PIN_2);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
/* Configuring the ADC sequencer (AND NOT TRIGGER!):-
* ->Use ADC0 (STEP 1)
* ->Use Sample Sequencer 1 (STEP 2)
* ->Ask the processor to trigger the sequence (STEP 3)
* ->Use the highest priority (STEP 4)
* # allow the ADC12 to run at its default rate of 1Msps
*/
ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_PROCESSOR, 0);
//Next we need to configure all four steps in the ADC sequencer
ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH0);
// Perform last step and set the interrupt flag (ADC_CTL_IE) as the last sample is done.
// Also, tell the ADC logic that this is the last conversion on SS1 (ADC_CTL_END)
ADCSequenceStepConfigure(ADC0_BASE, 1 ,3 ,ADC_CTL_CH0|ADC_CTL_IE|ADC_CTL_END);
//Enabling the SS1 (AND NOT TRIGGER!)
ADCSequenceEnable(ADC0_BASE, 1);
//An infinite loop
while(1)
{
//Read pin PE_2
i32Val = GPIOPinRead(GPIO_PORTE_BASE,GPIO_PIN_2);
GPIOPinRead(GPIO_PORTE_BASE, GPIO_PIN_3);
//Clearing the ADC interrupt status flag
ADCIntClear(ADC0_BASE, 1);
//Trigger the ADC conversion
ADCProcessorTrigger(ADC0_BASE, 1);
//Get the current Interrupt status | false indicates that "raw" interrupt status is reqd and not "masked"
//And wait until the status comes out to be 1 . i.e, the conversion is complete
while(!ADCIntStatus(ADC0_BASE, 1, false))
{ }
//Copy the ADC values from the SS1 into a buffer. SS1 -> (array)ui32ADC0Value
ADCSequenceDataGet(ADC0_BASE, 1, ui32ADC0Value);
ui32TempAvg = (ui32ADC0Value[0] + ui32ADC0Value[1] + ui32ADC0Value[2] + ui32ADC0Value[3] + 2)/4; //2 is for rounding
//TEMP = 147.5 – ((75 * (VREFP – VREFN) * ADCVALUE) / 4096) | We need to multiply everything by 10 to stay within the precision needed
ui32TempValueC = (1475 - ((2475 * ui32TempAvg)) / 4096)/10;
ui32TempValueF = ((ui32TempValueC * 9) + 160) / 5;
}
}