Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: TM4C1294NCPDT

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

Hi,

I am working in ti-rtos platform

Accidently comment the wdt reload time. Now controller is continuously resetting.

Now board is not detecting. Is there any way to out this issue.?

const WatchdogTiva_HWAttrs watchdogTivaHWAttrs[EK_TM4C1294XL_WATCHDOGCOUNT] = {
{
.baseAddr = WATCHDOG0_BASE,
.intNum = INT_WATCHDOG,
.intPriority = (~0),
//.reloadValue = 80000000 // 1 second period at default CPU clock freq

},
};

  • Hi,

     Since you comment out the reload, the reload register is just 0. Once you enable the WD the WD just keeps resetting since it times out immediately. You can do a mass erase of the device. Hope this method will help but no guarantee since you are forever resetting the device. Press the below "Unlock" button and follow the instruction on your launchPad. 

    1. Unpower the board and press reset

    2. Power the board but do not release the reset

    3. Run the unlock sequence according to the LM programmer "dialog box"

    4. Power Cycle the board 

    5. Do a Flash Erase Check or load a simple program to confirm the debugger can access the MCU again

  • Hi Charles,

    Thanks for your great and immediate support..

    Regards
    Nikhil