Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: TM4C1294NCPDT

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

Hi,

Is there any sample code available for internal eeprom in ti-rtos platform.

Regards

Nikhil

  • Hi Nikhil,

     Please refer to the TivaWare peripheral driver library user's guide for details. Below is a snippet of the example shown in the user's guide.

    The following example shows how to use the EEPROM API to write a block of data and read it back.
    uint32_t ui32EEPROMInit;
    uint32_t pui32Data[2];
    uint32_t pui32Read[2];
    //
    // Enable the EEPROM module.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_EEPROM0);
    //
    // Wait for the EEPROM module to be ready.
    //
    while(!SysCtlPeripheralReady(SYSCTL_PERIPH_EEPROM0))
    {
    }
    //
    // Wait for the EEPROM Initialization to complete
    //
    ui32EEPROMInit = EEPROMInit();
    //
    // Check if the EEPROM Initialization returned an error
    // and inform the application
    //
    if(ui32EEPROMInit != EEPROM_INIT_OK)
    {
    while(1)
    {
    }
    }
    //
    // Program some data into the EEPROM at address 0x400.
    //
    pui32Data[0] = 0x12345678;
    pui32Data[1] = 0x56789abc;
    EEPROMProgram(pui32Data, 0x400, sizeof(pui32Data));
    //
    // Read it back.
    //
    EEPROMRead(pui32Read, 0x400, sizeof(pui32Read));
    128

  • Thanks....

    Regards
    Nikhil