Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: TM4C1294NCPDT

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

Hi,

In the data sheet of tm4c1294ncpdt it mention that first timeout only generate interrupt and second timeout will generate the reset.

Is it possible to generate reset in the first timeout itself.

Regards

Nikhil

  • Ni Nikhil,

     No, it is not possible to generate reset in the first timeout.

    14.2 Functional Description
    The Watchdog Timer module generates the first time-out signal when the 32-bit counter reaches
    the zero state after being enabled; enabling the counter also enables the watchdog timer interrupt.
    The watchdog interrupt can be programmed to be a non-maskable interrupt (NMI) using the INTTYPE
    bit in the WDTCTL register. After the first time-out event, the 32-bit counter is re-loaded with the
    value of the Watchdog Timer Load (WDTLOAD) register, and the timer resumes counting down
    from that value. Once the Watchdog Timer has been configured, the Watchdog Timer Lock
    (WDTLOCK) register is written, which prevents the timer configuration from being inadvertently
    altered by software.
    If the timer counts down to its zero state again before the first time-out interrupt is cleared, and the
    reset signal has been enabled by setting the RESEN bit in the WDTCTL register, the Watchdog timer
    asserts its reset signal to the system. If the interrupt is cleared before the 32-bit counter reaches its
    second time-out, the 32-bit counter is