This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best Embedded controller for Bios (Intel/AMD X86) platform

Hi Team,

I would like to get the part number for an embedded controller with LPC support, so that I can interface with my Intel/AMD processor with it.

Platform is: Intel/AMD based Motherboard with all features of laptop/desktop.

but I have following concern on choosing the embedded controller.

1. it should support audio input (micro phone), stimulated audio support over spi is also fine ?.

2. embedded controller software support for integrating audio coded input (voice recognition). I can handle the audio input events in EC firmware/RTOS ?.

3. application circuits for interfacing audio microphone with embedded controller is there ?.

Please help me on this