Part Number: TM4C123GH6PM
Hello Community,
i tried to run the MCP23008 I2C I/O Expander using TM4C123. I simply only copied the code from the video:
TM4C123 Tutorial: I2C Communication (https://www.youtube.com/watch?v=A7PUM9wPUAw
/** * @author Carlos Alvarez (2/26/2015) * * @details Use the I2C peripheral in your Tiva-C or Stellaris Launchpad board * to drive an input output expander to control the state of 8 LEDs connected to * its GPIO port. * * See detail tutorial at: www.youtube.com/watch */ #include <TM4C123GH6PM.h> //#include <lm4f120h5qr.h> #include <stdbool.h> #include <stdint.h> #include "driverlib/timer.h" #include "driverlib/sysctl.h" #include "driverlib/interrupt.h" #include "driverlib/gpio.h" //#include "inc/hw_memmap.h" #include "inc/hw_ints.h" //I2C COMMUNICATION uint8_t leds = 0x00; uint32_t uiPeriod; void setSlaveAddress(uint8_t slaveAddress) { //MSA register consists of eight bits: 7 address bits and 1 Receive/Send bit, which determines if the next operation is Receive(1) or Transmit(0) //slaveAddress = 0b _001.0000 I2C1->MSA = (slaveAddress<<1); //Specify the slave address of the master } void setRW(uint8_t mode) { //NEXT operation is to Transmit if(mode == 0) { I2C1->MSA &= ~(1<<0); //Clear bit, transmitting data } else { I2C1->MSA |= (1<<0); //set bit, receiving data } } void writeByte(uint8_t dataByte, uint8_t conditions) { //This byte contains the data transferred during a transaction I2C1->MDR = dataByte; I2C1->MCS = conditions; while( (I2C1->MCS & (1<<0)) != 0); if( (I2C1->MCS & (1<<1) ) != 0) { if( (I2C1->MCS & (1<<4)) == 1){} else { I2C1->MCS = (1<<2); while( (I2C1->MCS & (1<<0)) != 0); } } } int main() { //Step 1 //Enalbe and provide a clock to I2C module 1 in Run mode. SYSCTL->RCGCI2C = (1<<1); //using I2C Module 1 //Step 2 SYSCTL->RCGCGPIO = (1<<0); //Module 1 uses port A => we must enable the clock on Port A //Step 3 GPIOA->AFSEL = (1<<6)|(1<<7); //Enabling the alternate functions for pin 6 and 7 GPIOA->DEN = (1<<6)|(1<<7); //They are digital signals //Step 4 //Setting a bit in this register enables the open-drain configuration of the corresponding GPIO pad //When this bit is enabled, it should also be set in the GPIODEN register. //PA7 corresponds to SDA. GPIOA->ODR = (1<<7); //Step 5 //GPIOA->PCTL &= ~0xFF000000; //This line is not required //Specify which alternate function you want to use, see Table 21-5 GPIOA->PCTL = (3<<28)|(3<<24); //put a 3 in PMC7 and PMC6 (pins PA7 and PA6 respectively) //Step 6 //Initialize I2C as a Master I2C1->MCR = (1<<4); //Master mode is enabled //Step 7 //Set the desired SCL clock speed of 100 Kbps //The TPR (for us is 7) is found using the formula on pg. 972 I2C1->MTPR = 0x7; //1 byte must be sent setSlaveAddress(0x20); //last 7 bits (7-1) setRW(0); //first bit (0) //writeByte(BYTE ONE, BYTE TWO) //send IODIR register address writeByte(0x00, (1<<0)|(1<<1)); //BYTE TWO: conditions = RUN and START //send IODIR value to make GPIO pins outputs writeByte(0x00, (1<<0)|(1<<2)); //BTYE TWO: conditions = RUN, STOP while(1) { writeByte(0x09, (1<<0)|(1<<1)); writeByte(0xFF, (1<<0)|(1<<2)); for(int i = 0; i < 1000000; i++){}; uiPeriod=SysCtlClockGet(); } return 0; }