This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6ZRB: CAN bus timing limitation between two messages

Expert 5120 points

Part Number: TM4C123GH6ZRB

Dear e2e Support,

My customer uses our TM4C123GH6ZRB in a one to one CAN architecture.

They've noticed that for a use at 500kbit/s, a 1ms delay is needed between two CAN messages of 100bits each.

Could you confirm if there is a hardware limitation from our side?

Their need is to go up to 3 messages per ms.

Regards,

besoin est d’aller jusqu’à 3 messages par ms.