Part Number: TMS570LC4357
Hello
we have problem with nError ping behavior during self tests.
In SPNS195C chapter 6.19 Error Signaling Module we found this information: "The nERROR can be used as an indicator to an external monitor circuit to put the system into a safe state."
OK, we are using this signal to put rest of system to "safe state". We are able to test ESM unit and this signal connection during boot (system is on safe state for booting). This signal can't be activated during normal operation later.
Problem is conflict with safety manual. For example SPNU540A chapter 7.133 Software Test of Parity Logic test ID "RAM13" (Table 4. Summary of Safety Features and Diagnostics) is marked as "Periodic / On-Demand". Problem is that this test can't be periodic, because this test activate nError signal every time. Is it correct? Can you clarify it?
Jiri