This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS/RM44L920: SCI TX/RX problem with DMA

Other Parts Discussed in Thread: RM44L920

Tool/software: Code Composer Studio

Hi,

I designed  communicate function between CPUs (RM44L920) though SCI, use DMA mode to send and receive data efficiently.  However,the DMA doesn‘t work when move the SCI Rd to the destination ram。

Here is my design:  connecting DMA request[30] , SCI receiver request to DMA CHANAN 0, while DMA request[31] , sci send request to DMA CHANNEL 1.

My control packets   are defined as following:

[SCI Rx] ---RD has received successfully, but DMA didn't move the RD to the destination ram.

SADD      = 0xfff7e538;  [RD]            /* source address             */
DADD      =  RamAdd;             /* destination  address       */
CHCTRL    = 0;                 /* channel control            */
FRCNT     = 1;                 /* frame count                */
ELCNT     = dsize;             /* element count              */

ELDOFFSET = 1;                 /* element destination offset */
ELSOFFSET = 0;                 /* element source offset */
FRDOFFSET = 1;                 /* frame destination offset   */
FRSOFFSET = 0;                 /* frame source offset   */

ADDMODERD = ADDR_FIXED;         /* address mode read, source  */
ADDMODEWR = ADDR_INC1;         /* address mode write ,dest   */

PORTASGN  = 4;                 /* port b                     */

RDSIZE    = ACCESS_8_BIT;     /* read size                  */
WRSIZE    = ACCESS_8_BIT;     /* write size                 */
TTYPE     = FRAME_TRANSFER ;   /* transfer type              */

 AUTOINIT  = AUTOINIT_OFF;       /* autoinit                   */

[SCI Tx] ---Sending data OK

SADD      = RamAdd;              /* source address             */
DADD      = 0xfff7e538;  [TD]            /* destination  address       */
CHCTRL    = 0;                 /* channel control            */
FRCNT     = 1;                 /* frame count                */
ELCNT     = dsize;             /* element count              */

ELDOFFSET = 0;                 /* element destination offset */

ELSOFFSET = 1;                 /* element source offset */
FRDOFFSET = 0;                 /* frame destination offset   */
FRSOFFSET = 1;                 /* frame source offset   */

ADDMODERD = ADDR_INC1;         /* address mode read,source   */

ADDMODEWR = ADDR_FIXED;       /* address mode write,dest    */

PORTASGN  = 4;                 /* port b                     */

RDSIZE    = ACCESS_8_BIT;     /* read size                  */
WRSIZE    = ACCESS_8_BIT;     /* write size                 */
TTYPE     = FRAME_TRANSFER ;   /* transfer type              */

 AUTOINIT  = AUTOINIT_OFF;       /* autoinit                   */

there are two question:
1. The registers of DMA channel 0/1,CSADDR/CDADDR/CTCOUNT, can't be showed in CCS
while the firmware is running. 
2. The DMA function of SCI sending data does work,but DMA function of SCI receiving data does't go well.
Note: the length of receiving data  isn't fixed every time.

Would you tell me how I could find the reason and solve it?

Best regards.

  • Hello,
    I will move this thread to the device forum. The device experts there can help you best.

    Thanks,
    ki
  • Hello,
    PLease, check source address (SADD) for receiving data, it should be Receiver Data Buffer address (FFF7 E534h).

    Best regards,
    Miro
  • Hi Miro,

    Thank you very much for your reply.

    As you say, the configured sadd is Receiver data buffer address(fff7e500).

    The function of DMA-SCI receive data does work when I set  both of 'RX DMA ALL' and 'RX DMA' 

    in SCI module.

    I am wondering whether the Rx DMA and Tx Dma of SCI can work simultaneously.

    So I would confirm it on board. Every time I set Rx DMA or Tx DMA when I need one of them.

    Best Regards.

    Yanbin Sun