Part Number: RM48L952
First, everything is OK,
Then, I downloaded modified firmware which has some bugs;
Finally, I can not downloaed firmware anymore.
When downloding firmware ,the error displayed is:
Fatal error: Failed to connect to the xds100 emulator(connect CPU)..
(Error -2062 @ 0x0)
Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/ or try more
reliable JTAG settings(e.g. lower TCLK).
(Emulation package 5.0.747.0)
any one can help me? Thanks a lot.