Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
I created a simple demo using the FreeRtos profile for HalCogen and compiled it using CC8.3.0.
The entirety of the code is here:
/** @file HL_sys_main.c
* @brief Application main file
* @date 07-July-2017
* @version 04.07.00
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2016 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
#include <stdio.h>
#include <FreeRTOS.h>
#include <os_task.h>
#include <os_queue.h>
#include <assert.h>
#include <HL_gio.h>
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
static QueueHandle_t tickQueue = NULL;
static uint32 LEDState = 0;
static void tickTask( void *pvParameters ) {
uint32_t val;
gioSetBit(gioPORTB,6,1);
for( ;; )
{
/* Wait until something arrives in the queue - this task will block
indefinitely provided INCLUDE_vTaskSuspend is set to 1 in
FreeRTOSConfig.h. */
xQueueReceive( tickQueue, &val, portMAX_DELAY );
gioSetBit(gioPORTB,7,LEDState);
LEDState = 1 - LEDState;
// printf("Val: %d\n",val);
}
}
/* USER CODE END */
uint8 emacAddress[6U] = {0xFFU, 0xFFU, 0xFFU, 0xFFU, 0xFFU, 0xFFU};
uint32 emacPhyAddress = 1U;
int main(void)
{
/* USER CODE BEGIN (3) */
gioInit();
printf("Startup!\n");
tickQueue = xQueueCreate( 10, sizeof( unsigned long ) );
assert(tickQueue);
BaseType_t stat = xTaskCreate( tickTask, /* The function that implements the task. */
"ticker", /* The text name assigned to the task - for debug only as it is not used by the kernel. */
configMINIMAL_STACK_SIZE, /* The size of the stack to allocate to the task. */
0, /* The parameter passed to the task - just to check the functionality. */
tskIDLE_PRIORITY + 1 , /* The priority assigned to the task. */
NULL ); /* The task handle is not required, so NULL is passed. */
assert(stat == pdPASS);
vTaskStartScheduler();
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
uint32_t count = 0;
uint32_t divider = 10;
void vApplicationTickHook( void ) {
count++;
if (count % divider == 0) {
xQueueSendFromISR( tickQueue, (void*)count, NULL );
}
}
/* USER CODE END */
The example runs for about 24 hours then hangs. Breaking into the execution brings me here:
resetEntry
b _c_int00
undefEntry
b undefEntry
b vPortSWI
prefetchEntry
b prefetchEntry
dataEntry
b dataEntry
b phantomInterrupt
ldr pc,[pc,#-0x1b0]
ldr pc,[pc,#-0x1b0]
;-------------------------------------------------------------------------------
The debugger highlights the "b dataEntry" line.
I set the tick rate on the OS config tab to 100Hz.
Any idea why this is happening?