Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi all,
I have a question about the TI documentation. I used the document spnu563.pdf (Technical Reference Manual for TMS570LC4357 Processor), Version May 2014.
Chapter 14.4.1 Clock Detect
The LPO HF clock frequency is typically near 9.6MHz, but ranges from 5.5MHz to 19.5MHz.
What does it mean a range from 5.5MHz to 19.5MHz ? Do you mean the LPO HF clock should ajust in HalCoGen between 5.5MHz - 19.5MHz ? Or do you mean if the LPO HF clock is set in HalCoGen to 9.6MHz it could be in a range from 5.5MHZ to 19.5Hz, may be for temperature reasons.
And is it possible to read out the actual LPO HF clock frequency ?
Best regards
Lars