Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software: Code Composer Studio
I'd appreciate any help here - trying to bring up a eval board from scratch using the pinmux tool and Tivaware. I currently can't get the basic program to compile when using the PinoutSet() function. I've included C:\ti\TivaWare_C_Series-2.1.4.178 and it's driverlib and inc subdirectories as separate search paths. Any suggestions?
Error/build messages:
**** Build of configuration Debug for project FirstTivaProgram ****
"C:\\ti\\ccs900\\ccs\\utils\\bin\\gmake" -k -j 8 all -O
Building file: "../main.c"
Invoking: ARM Compiler
"C:/ti/ccs900/ccs/tools/compiler/ti-cgt-arm_18.12.2.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/Users/Jack Bourne/Desktop/Tiva Programming/TivaSandbox/FirstTivaProgram" --include_path="C:/ti/TivaWare_C_Series-2.1.4.178/driverlib" --include_path="C:/ti/TivaWare_C_Series-2.1.4.178/inc" --include_path="C:/ti/TivaWare_C_Series-2.1.4.178" --include_path="C:/ti/ccs900/ccs/tools/compiler/ti-cgt-arm_18.12.2.LTS/include" --define=ccs="ccs" --define=PART_TM4C129ENCPDT -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
Finished building: "../main.c"
Building target: "FirstTivaProgram.out"
Invoking: ARM Linker
"C:/ti/ccs900/ccs/tools/compiler/ti-cgt-arm_18.12.2.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --define=ccs="ccs" --define=PART_TM4C129ENCPDT -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi -z -m"FirstTivaProgram.map" --heap_size=0 --stack_size=512 -i"C:/ti/ccs900/ccs/tools/compiler/ti-cgt-arm_18.12.2.LTS/lib" -i"C:/ti/ccs900/ccs/tools/compiler/ti-cgt-arm_18.12.2.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="FirstTivaProgram_linkInfo.xml" --rom_model -o "FirstTivaProgram.out" "./main.obj" "./pinout.obj" "./tm4c129encpdt_startup_ccs.obj" "../tm4c129encpdt.cmd" -llibc.a
<Linking>
undefined first referenced
symbol in file
--------- ----------------
GPIOPinTypeGPIOOutput ./pinout.obj
GPIOPinTypeUSBAnalog ./pinout.obj
GPIOPinWrite ./pinout.obj
SysCtlPeripheralEnable ./pinout.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "FirstTivaProgram.out" not built
>> Compilation failure
makefile:143: recipe for target 'FirstTivaProgram.out' failed
gmake[1]: *** [FirstTivaProgram.out] Error 1
makefile:139: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****
And the code:
#define TARGET_IS_TM4C129_RA2
//#include Pinmux files
#include "pinout.h"
//#include Tivaware libraries
#include <hw_adc.h>
#include <hw_can.h>
#include <hw_gpio.h>
#include <hw_ints.h>
#include <hw_pwm.h>
#include <hw_ssi.h>
#include <hw_uart.h>
#include <rom.h>
#include <rom_map.h>
//#include <tm4c129encpdt.h>
//#include standard C libraries
#include <stdint.h>
uint32_t hello_world;
uint32_t hello_world_max = 999999;
/**
* main.c
*/
void main(void)
{
////Processor setup////
//Processor Pin configuration (from pinmux tool)
PinoutSet();
//CAN Configuration
//SPI Configuration
////Peripheral setup////
//4-20 Transmitter Configuration
//4-20 Reciever Configuration
//Thermocouple Configuration
//Main infinite loop
for (;;)
{
for (hello_world = 1; hello_world <= hello_world_max; hello_world++)
{
}
}
}