Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Dear all,
I am using Tiva C TM4C1294NCPDT controller. I had downloaded the "boot_serial" example to the launchpad. After that via LM Flash Programmer i am able to download the app code.
My question is,
Some times while downloading the app code via LM Flash Programmer if any one of the following happens then not able to download the app code.
1. If power fails while the app code downloading or
2. Error / Timeout occurs while the app code downloading.
After downloading the bootloader code only, LM flash programming working to download the app code.
Any solution is available for this issue. i.e: if any disturbance occurs while app code download, then it needs boot loader code to continue further.
Pl. let us know if any solution is available or code modification is required?
Regards,
Iyyappan.V