Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
I'm new to using the Hercules board and am attempting to just run the following simple code: int main(void) { return 0; }
The board is connected to the computer via USB, and I do a clean build and debug. When I run it, the program stays in a busy loop in a function that's labeled as "ABORT - ABNORMAL PROGRAM TERMINATION. CURRENTLY JUST HALTS EXECUTION." led1, which is the error LED, also lights up.
I get the following output from the console:
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
I'm using CCS 9.0.1.
I'm not sure why I'm getting this error. Any help?