Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hello,
First off, this is probably not a huge deal and I can be missing something.
I am looking into ADC Calibration Mode and noticed that the first two equations in Table 19-1 Calibration Reference Voltages, seem to be flipped when I run adcCalibration in debug.
The math is right, but the order in which I expect them to show up is switch. Now I don't know if the HalcoGen code did something incorrect, or if there is an issue with the data sheet itself... or i just don't know how to read.
Overall, somewhere between Figure 19-11 and Table 19-1 and what I see in the debug from the HalcoGen code, something is swapped, but other than that, the data is good.
Best,
Ryan
INFO:
Windows 10
CCS: Version: 8.1.0.00011
HalcoGen: 04.07.00
Doc: spnu499c.pdf - section 19.8.1 - Figure 19-11 and Table 19-1